Interface IGpibIntfc
Description
The IGpibIntfc interface provides the properties and methods specific to GPIB INTFC sessions, except for messaging capabilities. These properties and methods tend to be an extension to the properties and methods present in the IGpib interface.
IGpibIntfc derives from IVisaSession.
Methods
|
Use of this method is discouraged. All the non-deprecated standard attributes are accessible via properties on the appropriate COM interfaces. |
|
|
Use of this method is discouraged. All the non-deprecated standard attributes are accessible via properties on the appropriate COM interfaces. |
|
|
Locks the resource. |
|
|
Unlocks the resource |
|
|
Opens the resource. This is the first method on IVisaSession or any of its derived interfaces to be called. In general, you will not call this method because you will use the Resource Manager to create resources. |
|
|
Closes the resource. Sending the resource's COM object's reference count to zero (and thus destroying the object) also executes a close, but this method may be useful for environments with garbage collection or other facilities that make object lifetimes non-deterministic. |
|
|
Writes GPIB command bytes on the bus. This operation attempts to write count number of bytes of GPIB commands to the interface bus associated with the session object. This operation returns only when the transfer terminates. |
|
|
Controls the state of the GPIB ATN interface line, and optionally the active controller state of the local interface board. This operation asserts or deasserts the GPIB ATN interface line according to the specified mode. The mode can also specify whether the local interface board should acquire or release Controller Active status. It is generally not necessary to use the ControlATN operation in most applications. Other operations such as Command and PassControl modify the ATN and/or CIC state automatically. |
|
|
Controls the state of the GPIB REN interface line and, optionally, the remote/local state of the device. This operation asserts or deasserts the GPIB REN interface line according to the specified mode. |
|
|
Tells the GPIB device at the specified address to become controller in charge (CIC). This operation passes controller in charge status to the device indicated by primAddr and secAddr, and then deasserts the ATN line. This operation assumes that the targeted device has controller capability. |
|
|
Pulses the interface clear line (IFC) for at least 100 microseconds. This operation asserts the IFC line and becomes controller in charge (CIC). The local board must be the system controller. |
Properties
|
A numeric version for this component. |
|
|
The VISA-defined version information for the specification version to which this component complies. |
|
|
The name of the hardware interface (GPIB, ASRL, etc.). |
|
|
The board number of the hardware interface. |
|
|
The type number of the hardware interface. |
|
|
The current locking state of the interface. |
|
|
The option string corresponding to the current state of the resource. |
|
|
The programmatic ID that can be used by COM to create this object. |
|
|
The VISA resource name of the currently open resource. This name is the canonical version of the resource name and therefore may vary from the resource string used to open/init the resource. |
|
|
The session type string, such as "INSTR" or "INTFC". |
|
|
The ID number of the vendor of this software component. |
|
|
The name of the vendor of this software component. |
|
|
The I/O timeout in milliseconds for I/O communication on this resource session. |
|
|
The return value from the last method call on this interface. This property may be useful in Visual Basic, where positive return values, such as warnings and other non-error return values, cannot be retrieved. See the Return Values page for a list of positive return values. |
|
|
Shows whether the specified GPIB interface is currently addressed to talk or listen, or is not addressed. |
|
|
Shows the current state of the GPIB ATN (ATtentioN) interface line. |
|
|
Specifies the 488-style status byte of the local controller associated with this session. If this property is set and bit 6 (0x40) is set, this device or controller will assert a service request (SRQ) if it is defined for this interface. |
|
|
Shows whether the specified GPIB interface is currently CIC (controller in charge). |
|
|
Specifies the total number of meters of GPIB cable used in the specified GPIB interface. If HS488 is not implemented, querying this attribute should return the value GPIB_HS488_NIMPL. On these systems, trying to set this attribute value will return the error E_VISA_NSUP_ATTR_STATE. |
|
|
Shows the current state of the GPIB NDAC (Not Data ACcepted) interface line. |
|
|
Primary address of the local GPIB controller used by the given session. |
|
|
Shows the current state of the GPIB REN (Remote ENable) interface line. |
|
|
Secondary address of the local GPIB controller used by the given session. |
|
|
Shows the current state of the GPIB SRQ (Service ReQuest) interface line. |
|
|
Shows whether the specified GPIB interface is currently the system controller. In some implementations, this attribute may be modified only through a configuration utility. On these systems, this attribute is read only (RO). |