IGpibIntfc::DevStatusByte

Description

Specifies the 488-style status byte of the local controller associated with this session.

If this property is set and bit 6 (0x40) is set, this device or controller will assert a service request (SRQ) if it is defined for this interface.

VB Prototype

Dim value As Byte
value = object.DevStatusByte

object.DevStatusByte = value

C++ Prototype

HRESULT get_DevStatusByte(
  BYTE* DevStatusByte
);

HRESULT put_DevStatusByte(
  BYTE DevStatusByte
);

Return Value

Refer to the table of return codes.

See Also

ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, AddressingState, ATNState, DevStatusByte, CICState, HS488CBLLength, NDACState, PrimaryAddress, RENState, SecondaryAddress, SRQState, SysControlState, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, Command, ControlATN, ControlREN, PassControl, SendIFC, IGpibIntfc Overview