IGpibIntfc::RENState
Description
Shows the current state of the GPIB REN (Remote ENable) interface line.
VB Prototype
Dim value As LineState
value = object.RENState
C++ Prototype
HRESULT get_RENState(
LineState* RENState
);
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, AddressingState, ATNState, DevStatusByte, CICState, HS488CBLLength, NDACState, PrimaryAddress, RENState, SecondaryAddress, SRQState, SysControlState, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, Command, ControlATN, ControlREN, PassControl, SendIFC, IGpibIntfc Overview