| Visual Basic (Declaration) | |
|---|---|
Public Overridable ReadOnly Property CarrierAggregation As CarrierAggregation | |
| C# | |
|---|---|
public virtual CarrierAggregation CarrierAggregation {get;} | |
| C++/CLI | |
|---|---|
public: virtual property CarrierAggregation^ CarrierAggregation { CarrierAggregation^ get(); } | |
Remote clients cannot select All; configure each carrier through ComponentCarriers. See CarrierAggregation for index mapping.
Measurement-level scalar settings address carrier 0 and, while All is selected in the user interface, also apply to every carrier. FrameCreationUtility, FbmcSettings, MulticarrierFilter, NomaSettings, and ScmaSettings address the carrier selected in the user interface, or carrier 0 while All is selected. To configure a specific carrier deterministically, use ComponentCarriers.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 31.00