Keysight 89600 VSA .NET API
HardwareInstrument Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : HardwareInstrument Class

Glossary Item Box

The following tables list the members exposed by HardwareInstrument.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyChassisGets the chassis number in which this instrument is located.  19.00
Public PropertyDriverRevisionGets the revision of the software driver used to communicate with the instrument.  —
Public PropertyExtraInfoGets the extra information for this instrument  22.00
Public PropertyFirmwareRevisionGets the revision of the firmware loaded in the instrument.  —
Public PropertyIdGets the InstrumentId of the instrument.  —
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyManufacturerGets the name of the manufacturer of the instrument.  15.00
Public PropertyModelGets the Model number of the instrument.  —
Public PropertyNameGets a descriptive name for the instrument.  —
Public PropertySerialNumberGets the serial number of the instrument.  —
Public PropertyServerPortNumberGets the server port number in which this instrument is located.  19.20
Public PropertySlotGets the slot number (if any) of the instrument.  —
Public PropertySubordinatesGets a collection of instruments that are subordinate to this instrument  24.20
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also