Keysight 89600 VSA .NET API
Associate Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Keysight.SA.Vsa Namespace > Mode Class : Associate Method


measurement
The measurement to associate with this Mode.

Glossary Item Box

Associates the supplied measurement with this Mode, so the Mode's shared configuration drives it (the measurement then appears in GetMeasurements and Agilent.SA.Vsa.Measurement.Mode resolves to this Mode).

Syntax

Visual Basic (Declaration) 
Public MustOverride Sub Associate( _
   ByVal measurement As Measurement _
) 
C# 
public abstract void Associate( 
   Measurement measurement
)
C++/CLI 
public:
abstract void Associate( 
   Measurement^ measurement
) 

Parameters

measurement
The measurement to associate with this Mode.

Remarks

A measurement belongs to at most one Mode. Associating it applies this Mode's current configuration without changing other measurements' associations.

This is the only way to change an association: once a measurement is under a Mode it stays under one, so move it by associating it with a different Mode of the same ConfigurationType.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also