Keysight 89600 VSA .NET API
ThresholdEventCondition Class
Members  See Also 
Agilent.SA.Vsa.Interfaces Assembly > Keysight.SA.Vsa Namespace : ThresholdEventCondition Class


Glossary Item Box

An EventCondition that checks an EventDataSource value to see if it meets certain thresholds.

Syntax

Remarks

This EventCondition supports multiple DataSources, but only from the same Agilent.SA.Vsa.Measurement. The same threshold will be applied to all values from the DataSources and if the value from any one of them satisfies the threshold, the Actions will be run.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 27.00

See Also

Reference

ThresholdEventCondition Members
Keysight.SA.Vsa Namespace
Keysight.SA.Vsa.EventRule.GetExtension``1
Keysight.SA.Vsa.EventRule.SetExtension``1