Keysight 89600 VSA .NET API
ThresholdEventCondition Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.Interfaces Assembly > Keysight.SA.Vsa Namespace : ThresholdEventCondition Class

Glossary Item Box

The following tables list the members exposed by ThresholdEventCondition.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyAbsoluteValueEnabledGets or sets a value indicating whether to take the absolute value of the data source before performing threshold comparisons.  —
Public PropertyComparisonPrecisionGets or sets the precision with which to make numerical comparisons between the thresholds and the value from the EventDataSource.  —
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyThresholdAGets or sets the value of the first threshold.  —
Public PropertyThresholdBGets or sets the value of the second threshold.  —
Public PropertyThresholdOperatorGets or sets a value indicating the operation to perform when comparing the ThresholdA and ThresholdB thresholds with the value from the EventDataSource.  —
Public PropertyThresholdOperatorNeedsAGets a value indicating whether the selected ThresholdOperator uses the value of ThresholdA.  —
Public PropertyThresholdOperatorNeedsBGets a value indicating whether the selected ThresholdOperator uses the value of ThresholdB.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCanUseDataSourceCheck whether this EventRule can use the specified type of EventDataSource (Inherited from Keysight.SA.Vsa.EventCondition)—
Public MethodCheckIfSatisfiedGets a value indicating whether the EventCondition is satisfied, based on the specified measurement's results. (Inherited from Keysight.SA.Vsa.EventCondition)—
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also

Reference

ThresholdEventCondition Class
Keysight.SA.Vsa Namespace
Keysight.SA.Vsa.EventRule.GetExtension``1
Keysight.SA.Vsa.EventRule.SetExtension``1