Keysight 89600 VSA .NET API
CyclicDelayDiversity Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > DownlinkUser Class : CyclicDelayDiversity Property


Glossary Item Box

Gets or sets the Cyclic Delay Diversity for the DL user.

Syntax

Visual Basic (Declaration) 
Public Overridable Property CyclicDelayDiversity As CyclicDelayDiversityType
C# 
public virtual CyclicDelayDiversityType CyclicDelayDiversity {get; set;}
C++/CLI 
public:
virtual property CyclicDelayDiversityType CyclicDelayDiversity {
   CyclicDelayDiversityType get();
   void set (    CyclicDelayDiversityType value);
}

Property Value

The default value is CyclicDelayDiversityType.WithoutCyclicDelayDiversity.

Remarks

This property is valid only if Precoding is SharedChannelDecoderType.SpatialMultiplexing.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 14.00

See Also