| Visual Basic (Declaration) | |
|---|---|
Public Overridable Property UersTransmitterPortNumber As AntennaPortType | |
| C# | |
|---|---|
public virtual AntennaPortType UersTransmitterPortNumber {get; set;} | |
| C++/CLI | |
|---|---|
public: virtual property AntennaPortType UersTransmitterPortNumber { AntennaPortType get(); void set ( AntennaPortType value); } | |
Property Value
The default value is AntennaPortType.Port5.This property is valid only in TDD mode.
This property is valid only if IsUersActive is true.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 14.00