Keysight 89600 VSA .NET API
FrequencyCenterUL Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : FrequencyCenterUL Property


Glossary Item Box

Gets or sets the center frequency of the UL signal, to be used to determine the limits for UL spectrum flatness test.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property FrequencyCenterUL As Double
C# 
public abstract double FrequencyCenterUL {get; set;}
C++/CLI 
public:
abstract property double FrequencyCenterUL {
   double get();
   void set (    double value);
}

Property Value

The default value is 1950 MHz (corresponding to the middle of E-UTRA operating band 1). The minimum value is FrequencyLowUL and the maximum value is FrequencyHighUL.

Remarks

Note that the value of this property can be different from the measurement center frequency.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 15.00

See Also