Get the phase offset of measurement input channel relative to the reference
InputChannel in degrees.
Syntax
Parameters
- inputChannel
- The measurement input channel for which the phase offset is being retrieved relative to the reference InputChannel
Return Value
The phase offset of the indicated measurement input channel in degrees relative to the reference
InputChannel
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 15.00
See Also