Keysight 89600 VSA .NET API
IsPuschHarqAckInformationSizeAutoDetected Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : IsPuschHarqAckInformationSizeAutoDetected Property


Glossary Item Box

Gets or sets a value indicating whether PUSCH HARQ-ACK Info Size Auto is enabled.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property IsPuschHarqAckInformationSizeAutoDetected As Boolean
C# 
public abstract bool IsPuschHarqAckInformationSizeAutoDetected {get; set;}
C++/CLI 
public:
abstract property bool IsPuschHarqAckInformationSizeAutoDetected {
   bool get();
   void set (    bool value);
}

Property Value

The default value is true.

Remarks

Please refer to associated property IsPuschHarqAckInformationSizeDynamic for details of the PUSCH HARQ-ACK Info Size auto-detection functionality supported when IsPuschHarqAckInformationSizeAutoDetected is true. Note, if the PUSCH HARQ-ACK Info Size content is known and 'static' (i.e. size is fixed or constant) for all PUSCH subframe allocations, then for best PUSCH decoding speed performance, we recommend setting IsPuschHarqAckInformationSizeAutoDetected value to false, and instead manually configure the appropriate PuschHarqAckInformationSize value.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also