Keysight 89600 VSA .NET API
ResultLengthAuto Property
See Also 
Agilent.SA.Vsa.NBIot.Interfaces Assembly > Agilent.SA.Vsa.NBIot Namespace > MeasurementExtension Class : ResultLengthAuto Property


Glossary Item Box

Gets or sets a value indicating whether ResultLength is determined based on other parameters (uplink-only).

Syntax

Visual Basic (Declaration) 
Public MustOverride Property ResultLengthAuto As Boolean
C# 
public abstract bool ResultLengthAuto {get; set;}
C++/CLI 
public:
abstract property bool ResultLengthAuto {
   bool get();
   void set (    bool value);
}

Remarks

Currently supported for NPUSCH. Result Length is calculated based on Npusch.RUNumber, Npusch.Repetitions, and Npusch.StartSubframe.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 24.00

See Also