Keysight 89600 VSA .NET API
CarrierAggregation Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : CarrierAggregation Class

Glossary Item Box

The following tables list the members exposed by CarrierAggregation.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyAllowMultipleCarrierDefinitionsGets or sets a value indicating whether all carriers use the same Carrier Definition or not.  24.20
Public PropertyCarrierMappingsGets a reference to the collection of carrier mapping settings.  24.20
Public PropertyComponentCarriersGets a reference to the collection of Carrier Definitions.  24.20
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyLinkDirectionGets or sets the link direction of the carrier aggregation scheme.  24.20
Public PropertyReferenceCarrierGets or sets the component carrier used as a reference for cross-carrier measurement results.  —
Public PropertyResultCarrierIndexGets or sets the zero-based component carrier index to indicate the component carrier used for the measurement result display.  24.20
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodConfigureConfigures the mappings, reference carrier, measurement channel mappings, and frequency span to simplify setting up certain carrier aggregation scenarios.  —
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also