Keysight 89600 VSA .NET API
Coreset Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : Coreset Class

Glossary Item Box

The following tables list the members exposed by Coreset.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyAllocatedRBGroupsGets or sets allocated REGs  —
Public PropertyAllocatedRBGroupsMsbGets or sets allocated RB Groups in most significant bit order  —
Public PropertyBwpIdGets or sets BWP Id  24.20
Public PropertyCceToRegMappingTypeGets or sets coreset CCE to REG mapping type  —
Public PropertyCoreset0RBNumberGets or sets a value indicating the number of resource blocks assigned to CORESET0.  24.20
Public PropertyCoreset0RBOffsetGets or sets a value indicating the start index of resource block assigned to CORESET0.  24.20
Public PropertyCoresetIdGets or sets the coreset ID for this coreset instance.  24.00
Public PropertyDmrsScramblingIdGets or sets DMRS Scrambling Id  24.20
Public PropertyInterleaverSizeGets or sets interleave size.  —
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyPrecoderGranularityGets or sets coreset precoder granularity  24.00
Public PropertyRBOffsetR16Gets or sets a value indicating the rb-Offset-r16 configured for this CORESET.  25.40
Public PropertyRBOffsetR16ConfiguredGets or sets a value indicating whether rb-Offset-r16 is configured or not.  25.40
Public PropertyRegBundleSizeGets or sets REG bundle size.  —
Public PropertyShiftIndexGets or sets shift index.  —
Public PropertyShiftIndexSourceGets or sets a value indicating whether the Shift Index value used for is configured by higher layer or from cell ID.  24.20
Public PropertySymbolNumberGets or sets the core-set symbol number.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetAllocatedRBGroupIndexesGets the set of RB groups indexes allocated for this coreset.  —
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodSetAllocatedRBGroupIndexesOverloaded. Sets a single contiguous set of RB groups to be allocated for this coreset.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also