Keysight 89600 VSA .NET API
Prs Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : Prs Class

Glossary Item Box

The following tables list the members exposed by Prs.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyBwpIdGets or sets the Id of the BWP where this physical channel is scheduled  29.40
Public PropertyCombSizeGets or sets a value indicating the comb size.  29.40
Public PropertyEnabledGets or sets a value indicating whether the physical channel is marked as enabled.  29.40
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyNameGets a value for the name for the physical channel.  29.40
Public PropertyPointAOffsetInSubcarrierGets or sets a value indicating the PointA Offset in subcarriers.  29.40
Public PropertyPowerBoostingGets or sets a value indicating the relative power boosting (in dB) with this physical channel.  29.40
Public PropertyRBNumberGets or sets a value indicating the number of resource blocks assigned to the physical channel.  29.40
Public PropertyRBOffsetGets or sets a value indicating the start index of the resource block assigned to the physical channel.  29.40
Public PropertyResourceSetGets a reference to Resource Set settings.  29.40
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also