Keysight 89600 VSA .NET API
Rimrs Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : Rimrs Class

Glossary Item Box

The following tables list the members exposed by Rimrs.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyEnabledGets or sets a value indicating whether this physical signal is marked as enabled.  —
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyIsIncludedInRmsEvmGets or sets a value indicating whether Rimrs is included in RMS EVM calculation/>.  24.20
Public PropertyL0SymbolIndexGets or sets a value indicating the L0 symbol index in a slot used by this physical signal.  —
Public PropertyNscidGets or sets a value indicating the SCID value used for sequence generation.  —
Public PropertyNumberOfRBsGets or sets a value indicating the number of resource blocks assigned to this physical signal.  —
Public PropertyNumberOfTransmissionPeriodsGets or sets a value indicating the number of RIM-RS transmission periods.  —
Public PropertyNumerologyGets or sets a value indicating the numerology for this physical signal.  —
Public PropertyPowerBoostingGets or sets a value indicating the relative power boosting (in dB) of this physical signal.  —
Public PropertyRBStartIndexGets or sets a value indicating the start index of resource block assigned to the physical signal.  —
Public PropertySequenceMultiplierFactorGets or sets a value indicating the multiplier factor used in sequence generation.  —
Public PropertySequenceOffsetGets or sets a value indicating the sequence offset used in sequence generation.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetAllocatedSlotIndexesGets the set of slot indexes allocated for this physical signal.  —
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodSetAllocatedSlotIndexesOverloaded. Sets a single contiguous set of slots to be allocated for this physical signal.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also