Keysight 89600 VSA .NET API
SSBlock Class Properties
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : SSBlock Class


Glossary Item Box

For a list of all members of this type, see SSBlock members.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyActiveIndexesGets or sets the indexes (zero-based) on which the SS/PBCH physical channels are reserved.  
Public PropertyAutoDetectActiveBlocksOnGets or sets a value indicating whether to auto detect which SS/PBCH blocks are active.  
Public PropertyAutoDetectPowerThresholdGets or sets the power threshold (in dB, relative to maximum SS/PBCH block power) to use to decide if an SS/PBCH block is active.  
Public PropertyHalfFrameIndexGets or sets the value indicating the half frame index the SSB block starts with when the SSB block period is not 5 milliseconds.  26.00
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)
Public PropertyIsSSBlockEnabledGets or sets a value indicating whether this resource allocation is currently applied to the ComponentCarrier .  
Public PropertyLmaxGets or sets the maximum number of possible SS/PBCH blocks in a transmission opportunity.  
Public PropertyNumerologyGets or sets a value indicating the numerology for this resource allocation.  
Public PropertyPbchGets a reference to the PBCH physical channel settings.  
Public PropertyPeriodicityGets or sets a value indicating the SS/PBCH resource allocation periodicity.  
Public PropertyPssGets a reference to the PSS physical channel settings.  
Public PropertyRBNumberGets a value indicating the number of RB available in this resource allocation.  
Public PropertyRBOffsetGets or sets a value indicating the RB Offset for this resource allocation.  
Public PropertySssGets a reference to the SSS physical channel settings.  
Public PropertySubcarrierOffsetGets or sets the subcarrier offset of the SS/PBCH block relative to the RBOffset.  
Public PropertySubcarrierSpacingCommonGets or sets the subcarrier spacing used for the SubcarrierOffset when ssb numerology is 120kHz or 240kHz.  24.20
Public PropertySymbolStartForMu1Gets or sets the symbol start equation used when the numerology is 30 kHz (µ = 1)  
Public PropertyVersionGets or sets the specification interpretation to use for SS/PBCH.  
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also