For a list of all members of this type, see AngleOfArrival members.
Name | Description | Minimum SW Version | |
---|---|---|---|
![]() | AnalysisMode | Gets or sets a value indicating the analysis mode used to calculate the angle. | — |
![]() | AntennaOrientation | Gets or sets a value indicating the antenna orientation to use. | — |
![]() | Antennas | Gets a reference to the AoaAntennaCollection. | — |
![]() | AntennaSpacing | Gets or sets a value indicating the antenna spacing to use for each AoaAntenna. | — |
![]() | Enabled | Gets or sets a value indicating whether angle of arrival analysis is enabled. | — |
![]() | FrequencyReference | Gets or sets a value indicating the frequency reference used to calculate the angle. | — |
![]() | IsDisposed | Gets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
![]() | ManualReferenceFrequency | Gets or sets a value indicating the manual reference frequency used to calculate the angle. | — |
![]() | TdoaMode | Gets or sets a value indicating the timing reference of TDOA. | — |
‡ This is the minimum 89600 VSA software version level needed to use this member. |