Spectrum (802.16 OFDM)
The trace data shows the frequency spectrum of the trace. When Demodulation is enabled, the trace is the averaged, Inst Spectrum display, as shown in the following block diagram. If averaging is off, the and displays are identical.
The trace has the following characteristics:
-
It is derived from pre-demodulated time data, which is usually 20% larger than the result length. See Time.
-
It is averaged if averaging is ON and the average type is rms, rms exponential, or peak averaging.
If averaging is ON, a scan is not included in the average if any of these conditions exist: Pulse Not Found, Sync Not Found, Carrier Unlock, or certain DATA? conditions.
VSA signal flow (see Digital Demodulation Block Diagram):
See Also