UL-MAP Decoding (802.16 OFDMA)
: Selected (See OFDMA Standard Presets Table.)
(applies to only)
When the VSA is set to analysis mode, will decode the UL Up Link (reverse link: from cell phone to base station)-MAP messages of the downlink subframe when a UL-MAP exists and report the interpreted results in the UL-MAP Info trace. will accommodate Normal or Compressed mode UL-MAP messages encoded with either CC (convolutional coding) or CTC (convolutional turbo coding) encoders. The DL-MAP Decoding property must be selected for to be available.
: Automatic UL-MAP decoding is performed.
: Automatic UL-MAP decoding is not performed.
The VSA also provides DL-MAP Decoding.
See Also