Subcarrier Interval (802.16 OFDMA)
: 1 (See OFDMA Standard Presets Table.)
specifies the range of subcarriers in the subset that will be analyzed when the VSA is set to Uniform Data Analysis mode.
is only available when the on the tab is cleared.
See Also