Subcarrier Offset (802.16 OFDMA)
: 1 (See OFDMA Standard Presets Table.)
specifies the first subcarrier of the subset of subcarriers when the VSA is set to Uniform Data Analysis mode.
is only available when the on the tab is cleared.
See Also