Override Preamble Definition (802.16 OFDMA)
: Cleared (See OFDMA Standard Presets Table.)
(applies to only)
allows manual setting of the IDCell and Segment parameters.
-
(manual mode): The VSA uses the and text box values.
-
(auto mode): The VSA ignores the and text box values and uses internal preset values based on the Preamble Index value and table 309 of the IEEE Institute of Electrical and Electronics Engineers. A US-based membership organisation that includes engineers, scientists, and students in electronics and related fields. The IEEE developed the 802 series wired and wireless LAN standards. Visit the IEEE at http://www.ieee.org 802.16e standard.
See Also