Downlink (Subframe Type) (802.16 OFDMA)
: Selected (See OFDMA Standard Presets Table.)
Subframe Type sets the VSA to Downlink analysis mode. The VSA will demodulate and analyze the downlink subframe within the current OFDMA analysis frame. (Applies to both Uniform Zone analysis and Data Burst Analysis modes).
1) When is selected, all downlink specific demodulation properties will be made active and all demodulation properties will be made inactive (greyed).
2) To measure the Uplink subframe, set the VSA to Uplink Subframe Type.
Some Subframe Type specific parameters are (only available when is selected):
See Also