IDCell (802.16 OFDMA)
: 0 (See OFDMA Standard Presets Table.)
(applies to only)
specifies the starting IDCell value for the frame. The Preamble Index value and the subframe Downlink Override Preamble Definition setting determines what IDCell value is used by the VSA.
IDCell may determine the DL_Permbase
If the Override IDCell with PermBase parameter ( tab) is selected, the DL Down Link (forward link: from base station to cell phone)_ value is forced to match the IDCell value (which may be derived from the ).
See Also