Override Measurement Region (demodulation) (802.16 OFDMA)
: Cleared (See OFDMA Standard Presets Table)
manually specifies a "zoomed" measurement analysis region and also changes or adds additional time domain data to the trace and computed trace results. enables the following parameters:
Enable additional demodulator settings must be selected for to be available.
The is referenced to the start of the defined zone.
See Also