Selected Burst (802.16 OFDMA)
The text box specifies the burst to define and is used to rename the burst. When a burst is selected in the Bursts in Selected Zone list box, the name will be displayed in the text box.
To rename a burst, click in the text box and type in desired name.
The following parameters are used to define a selected burst:
- Definition Type
- Allocation Geometry
- Data Tone Modulation
- Boosting Level (Downlink only)
- STC Mode (Uplink only)
- Pilot Pattern (Uplink only)
See Also