IEEE 802.16 OFDMA Demod Properties Dialog Box

The IEEE 802.16 OFDMA Demod Properties dialog box contains all the parameters and functions required to configure the VSA to demodulate and analyze 802.16 OFDMA modulated signals.

The 802.16 OFDMA demodulator must be selected before this dialog box is available. To enable the demodulator, click Analysis > Demodulator > Wireless Connectivity > IEEE 802.16 OFDMA.

The IEEE 802.16 OFDMA Demod Properties dialog box contains these tabs: