Region Table (Advanced-Radar/Hopping)
Menu Path:
Region Table metrics are only available when the Phase, Frequency or Linear Chirp Synchronization Domain is selected.
The Region Table is a type of Matrix Table that includes all region-specific result metrics, measured over all valid region time samples detected within the user-defined Acquisition Length (sec) up to the Max Detection Count value specified in the Region panel.
Region Table metrics are listed under the following groupings:
- Pulse
- Region
- Time/Level
- Settling
- Phase Modulation
- Frequency Modulation
- Chirp Modulation
- Best-Fit FM
- PM Error
- FM Error
- Chirp Error
Sorting by metric
You can sort the table by any metric by left-clicking the metric name. Click again to toggle between ascending or descending order. Cancel sorting by right-clicking and selecting "Clear Sort".
You can highlight one row, then right-click and select Set Start Region to conveniently set the Starting Region.
See Also