All Data Streams Active (Custom OFDM)
specifies whether all Data type allocations within the Resource Map are assumed to be active on all MIMO Multiple Input, Multiple Output: A physical layer (PHY) configuration in which both transmitter and receiver use multiple antennas. antenna associated data streams.
Selected (default) - For MIMO demodulation, each Data type allocation within the Resource Map is assumed to be active on all MIMO antenna associated data streams.
Cleared - For MIMO demodulation, the mapping of each Data type allocation within the Resource Map to MIMO antenna associated data streams is determined using the combination of 1-bit Multiple Antenna value and/or the 3-bit Antenna Index value defined within the Resource Map. For this case, a given Data type allocation within the Resource Map is assumed to be active on all MIMO antenna associated data streams only if the 1-bit Multiple Antenna value is set to true. Otherwise, the given Data type allocation is assumed to be active only on the MIMO antenna data stream associated with the 3-bit Antenna Index value.
The All Data Streams Active checkbox is cleared (set to false) during execution Apply Frame Definition process, since it includes writing the specified Multiple Antenna and Antenna Index values into the generated Resource Map.
See Also