MIMO Configuration (Custom OFDM)
MIMO Multiple Input, Multiple Output: A physical layer (PHY) configuration in which both transmitter and receiver use multiple antennas. Configuration contains parameters that specify the allocation's antenna port mapping definitions.
(Allocation Type set to either Pilot or Preamble) - Specifies a single antenna port index to which the allocation is mapped.
Range: 0 to (Transmitter Antennas - 1)
(Allocation Type set to either Data or Idle) - Specifies the indexes of the active antenna port(s) that are mapped to the allocation. Enter the port indexes as a comma-separated list. Use a colon (:) to indicate a range of ports.
Range: 0 to (Transmitter Antennas - 1)
See Also