CP/CS Repeat Index (Custom OFDM)

Analysis > Custom OFDM Demod Properties > Format tab

This parameter is shown in the Frame Definition tab and the Format tab. When Frame Definition > Apply is clicked, the value in the Frame Definition tab is applied to the Format tab (and the signal).

CP/CS Repeat Index specifies the cyclic prefix and cyclic suffix (also referred to as guard interval) repeat index - If the Cyclic Prefix/Suffix (Ratio) Per Symbol arrays are at least as long as the measurement result length, it provides a cyclic prefix/suffix value for each symbol. If the array is shorter than the measurement result length, processing loops back and re-uses the array (and keeps looping back every time the end of the array is reached again). The location within the array that is looped back to is determined by the CP 1) Contention period, or 2) Cyclic prefix Repeat Index. For clarity in the explanation below, let RepeatIndex equal the CP/CS Repeat Index, and ArrayLength equal the length of the Cyclic Prefix/Suffix (Ratio) Per Symbol arrays. There are four possible cases:

See Also

Format Tab

Custom OFDM Demod Properties