Resource Map Repeat Index (Custom OFDM)

Analysis > Custom OFDM Demod Properties > Format tab

This parameter is shown in the Frame Definition tab and the Format tab. When Frame Definition > Apply is clicked, the value in the Frame Definition tab is applied to the Format tab (and the signal analysis results).

 Default: 0 Symbols

Resource Map Repeat Index sets how to loop back if the end of the Format tab resource mapping array properties (i.e. Resource Map, Resource Modulation and Resource Allocations) is reached. If the resource mapping array properties are shorter than the result length, then this parameter specifies where to loop back to within the resource mapping array properties after the end is reached. The value is specified in terms of symbol number. For example, a value of zero means that the analyzer loops back to the beginning of the resource mapping array properties, while a value of one means that the analyzer loops back to the second symbol of the resource mapping array properties.

See Also

Custom OFDM Demod Properties