Time Gap Repeat Index (Custom OFDM)

Analysis > Custom OFDM Demod Properties > Format tab

This parameter is shown in the Frame Definition tab and the Format tab. When Frame Definition > Apply is clicked, the value in the Frame Definition tab is applied to the Format tab (and the signal analysis results).

Default: 0

Time Gap Repeat Index - If the Time Gap array is at least as long as the measurement result length, it provides a time gap value for each symbol. If the array is shorter than the measurement result length, processing loops back and re-uses the array (and keeps looping back every time the end of the array is reached again). The location within the array that is looped back to is determined by the Time Gaps Repeat Index. This repeat index works the same way as the CP 1) Contention period, or 2) Cyclic prefix/CS Repeat Index works with the Cyclic Prefix/Suffix (Ratio) Per Symbol arrays.

See Also

Time Gaps

Custom OFDM Demod Properties