Auto Detect Setup

Menu Path: Analysis > FMCW Radar Properties > Reference Synchronization

Auto-Detect Setup parameters are used to describe which valid LFM regions within the signal to automatically detect, synchronize to, and include within the FMCW region analysis results.

The Auto-Detect Setup parameters are only valid when Region Synchronization is set to Automatic.

The illustration below shows Auto-Detect Setup used to select which LFM regions are valid. In this example:

See Also

FM Slope Threshold

Reference Region Count

First Region FM Slope

FM Filter Bandwidth

Max Region FM Slope Deviation