Manual Reference Description

Menu Path: Analysis > FMCW Radar Properties > Reference Synchronization

Manual Reference Description parameters are used to describe the ideal reference signal LFM region-group pattern which repeats within the measured signal's FM Frequency Modulation Slope (Hz/us) modulation.

The Manual Reference Description settings DO NOT appear when See "Region Synchronization" is Automatic.  Region Synchronization must be set to Sync to Manual Reference or Triggered to access these settings.

These reference description parameters are used for both Sync to Manual Reference and Triggered Region Synchronization modes, as follows:

Adding and Removing Regions

You use the Add Region button to add a new Reference Region index to the Manual Reference Description. You use the Remove Region button to remove the last Reference Region index from the Manual Reference Description.

Editing Manually Defined Reference Regions

The Edit button opens an editor that allows you to make multiple changes to the manually defined reference regions without needing a measurement update each time you change a parameter.

For each Reference Region, you can specify:

Specifying Frequencies

You can define Manual Reference Description frequencies as either relative or absolute Hz values.

Default: Frequencies are Relative to Measurement Center

See Also

Input Trigger

Copy Auto to Manual