Trace Scale Tab

From the Trace Scale tab in the Spectrogram dialog box the time length of the spectrogram viewport can be changed, as well as where this viewport is located in the trace buffer. The parameters include:

The area to the left of the spectrogram can be right clicked and Trace Scaleselected to open the Trace Scale tab.

See Also

Spectrogram / Color Map Tab

About Spectrograms