Y-Axis Popup Menu

Right-clicking near the Y-axis opens the Y-axis popup menu, which lets you modify frequently used Y-axis parameters.

Y Auto Scale performs a Y-axis autoscale the trace (same as clicking the Y Auto Scale button in the Trace > Y Scale tab).

Y Scale displays the Y Scale tab (same as clicking Trace > Properties > Y Scale from the main menu), which chooses Y-axis units, sets the reference level or reference position, and sets other Y-axis parameters.

Format displays the Format tab (same as clicking Trace > Format from the main menu), selects trace coordinates.

Coupling displays the Coupling tab (same as clicking Trace > Couplingfrom the main menu), selects coupling with overlaid traces.

Average displays the Average tab (same as clicking Trace > Averagefrom the main menu), selects trace averaging.

Trace Auto Scale clears Fixed Height so that each horizontal trace line in the spectrogram is one pixel high and also clears Trace Offset in the Spectrogram Trace Scale Tab.

Trace Scale changes the time (vertical axis) scaling of the spectrogram trace.

Select this Measurement selects the measurement to which this trace belongs.