Preset Application and Traces
presets everything listed in these preset options. For a list of the parameters set by each preset function, see the following:
In addition to the parameters listed for each of the above functions, also performs these functions:
- Input Channels configuration is set to 1 Channel.
- All Demodulator settings (in the dialog box) are set to default.
- Calibration (User Correction , Fixed Equalization, and Frequency Reference) settings are set to default.
Preset Application and Traces never changes the hardware setup, Startup Preferences, General Preferences, Display Preferences or SCPI Preferences.