Playing a Recording
-
Play the recording:
-
Click the button on the Control toolbar.
OR
-
Click (from the main menu)
-
-
Set up Playback Trigger, if necessary.
The can also be used to play a recording. The also contains controls and indicators that choose what section of the recording to play back. For more information, see Using the Player.
Different values can be used for overlap processing to control the speed of the playback. Higher values slow the playback, lower values increase playback speed.
Time Corrections and Playing a Recording
Time-domain corrections are applied permanently to recordings as they are saved in any file format except SDF (Fast) format. This includes any calibration that was selected by the user at the time the signal was recorded. Correcting in this manner allows the user to save fully-corrected data for further processing using MATLAB or other mathematical software. When you recall and playback a recording, the current self-calibration and external corrections are not applied. The External Amplitude tab and External Frequency tab calibration parameters are disabled (greyed-out) during recording playback.
For recordings saved in SDF (Fast) format, the data is saved uncorrected, but correction data is saved with the time data. This correction is applied when the time data is played back. The tab sections are disabled (greyed-out) during recording playback.
For more information, see About User Correction.
I+jQ Measurements and Playing back a Recording
Signals that are recorded in I+jQ mode should be played back in I+jQ mode. While they can be played back as 2 or 4 (Dual I+jQ) separate channels, the time corrections will not in general be consistent. 2-channel or 4-channel Baseband recordings, however, can be played back in I+jQ or Dual I+jQ mode and time corrections will be accurate.
Segmented Recordings
For segmented recordings, the shows the start and stop times as if the segmented recording were one segment. The Player does not know about segment start times and boundaries. Therefore, the stop time is:
- SegmentXDelta * (Number of Points in Y data)
Using Overlap Processing On a Digitally Pulsed Signal
If playing back a pulsed, digitally modulated signal and using digital demodulation with pulse search to demodulate the signal, note that overlap processing uses the search length to determine the amount of overlap, not the result length. The search length determines how much data is collected whereas the result length determines how much data is demodulated and displayed.
The Recording and Playback feature is not available with Power Spectrum measurements.