X Per Division (X Scale)
(applies only to Real vs. Imag trace format)
defines the spacing between horizontal divisions (denoted by graticule lines when Show Grid Lines is enabled). Increase to show more data in the trace grid (and reduce the resolution); decrease to show less data in the trace grid (and increase the resolution).
can be changed by clicking that hotspot in the trace window.
See Also