Range Tracking (Y Scale)
When the check box is selected, range tracking is enabled for the active trace. When the check box is cleared, range tracking is disabled.
When range tracking is on, the value of Reference Level is linked to the input range. Each time the range changes, changes by the same amount.
Range tracking is disabled during a Y Auto Scale or Trace Auto Scale procedure or when the Y Per Division is changed. Range tracking is only available for certain, pre-demod trace data including Auto Correlation, Gate Time, Inst Main Time, Inst Spectrum, and Spectrum traces.
Range tracking is not available for these types of measurement data:
- Any post-demod trace data
- Math functions
- Data registers (includes recalled traces)
- Frequency response
- Coherence
Range tracking is not supported for these trace formats:
- Wrap or Unwrap Phase
- Group Delay
- Trellis-Eye
- Real vs. Imag
See Also