Gate Time (Trace Data)
trace data displays the selected channel's gate time-record.
is only available when the measurement type is .
When time gating is on, displays the portion of the main time-record marked by the gate--this portion is called the gate record (when time gating is off, displays nothing).
As a reminder, when time gating is on, the VSA uses the gate time-record to compute frequency information such as spectrum, frequency response, coherence, and correlation.
See Also