Exclude TX Settling Time (802.15.4 HRP UWB)
The parameter group tells the demodulator to ignore part of the SHR, from the beginning of the frame to the excluded settling time.
The excluded part of the SHR is shown in the IQ Meas Time, IQ Ref Time and Error Vector Time traces.
On the traces that display Vect: NNN averaging (Eq Impulse Response, Ch Frequency Response, and RRC Correlated), the Vect: NNN averaging notation shows the actual number of SYNC symbol repetitions that are averaged to compute the trace. The Exclude TX Transmit or transmitter Settling Time is rounded up to an integer number of repetitions, and this number of repetitions is excluded from the average.
- excludes the specified time from the beginning of SHR when computing the NRMSE for SHR. Does not affect the amount of SHR used to estimate impairments.
Default: 0 s
- excludes the specified time from the beginning of SHR when estimating the frequency error, phase offset, chip clock error, and phase tracking corrections.
Default: 15 µs
See Also