Duplex Mode (LTE-Advanced)
FDD Frequency Division Duplex: A duplex scheme in which uplink and downlink transmissions use different frequencies but are typically simultaneous.
configures the demodulator to demodulate either FDD (frame type 1) or TDD (frame type 2) signals.
The selection is enabled by Opt. BHG, and the selection is enabled by Opt. BHH. Duplex modes that are not licensed will be grayed out and not selectable.
While most parameters can be set differently for each component carrier, this parameter is required to be the same across all component carriers.
There are some differences in the dialog when is selected. See the following topics for more information:
- The Format tab will show two parameters specific to TDD mode: Dw/GP/Up Len and UL/DL Config.
- The Advanced tab contains several TDD only parameters.
- Downlink Control Channel Properties (, )
- LTE Allocation Editor (TDD-only parameters: , , , , , , PRACH Physical Random Access Channel )
See Also
LTE-Advanced Demod Properties Dialog Box