Preset to Standard (LTE)
sets the demodulator to the specified bandwidth and configures the settings for all tabs in the LTE-Advanced Demod Properties dialog, except the Common tab, for component carrier x according to the default values listed in Using a Standard Setup for the current direction (or ).
Parameters not specific to the current direction are not changed. For example, when is set to downlink and the demodulator is preset to standard, uplink user allocations in the LTE Allocation Editor are left intact and will still be available when is switched back to uplink.
See Also
Setting up an LTE-Advanced Measurement