Result Length (LTE-Advanced)
20 slots or the length of the signal, whichever is larger
determines how many slots will be available for demodulation. Measurement Interval and Measurement Offset specify which part of the time capture is demodulated.
While most parameters can be set differently for each component carrier, this parameter is required to be the same across all component carriers.
The result data starts where the analysis boundary is found and ends after the amount of data specified by .
The length of the time capture (contained in Search Time) is longer than the result length by approximately the length of the Analysis Start Boundary (frame = 10 ms, slot = 0.5 ms, etc.) to allow for location of the analysis boundary within the time capture.
For downlink, an entire slot containing S-SS Secondary Synchronization Signal must be present in the time capture (Raw Main Time) for demodulation to occur.
See Also