PUSCH allocations (LTE)
This topic contains a information on configuring the PUSCH Physical Uplink Shared Channel channel allocations for a user mapping. There are two sections, one for configuring PUSCH for resource block autodetection, and one for manually defining PUSCH resource block allocations.
To set up a user mapping, see the Uplink user allocations topic.
For more information about the parameters listed in the procedure below, see the LTE Allocation Editor topic.
Configuring PUSCH for resource block autodetection
-
Select the tab
-
Configure frequency hopping
-
Set frequency hopping type ()
- Specify whether to use or frequency hopping ()
-
Set the frequency hopping offset ()
-
Set the number of frequency hopping subbands ()
-
-
Configure DMRS parameter auto-calculation
-
Select
-
Set
-
Set
-
Set
To specify uniform DMRS parameters, clear the parameter and set , , and per-slot parameters. These DMRS parameter will apply to all PUSCH resource block allocations found in the frame.
-
-
Configure sync slot
Skip to Step 5 if you have chosen a different signal than PUSCH DMRS for synchronization. The demodulator will ignore the sync slot parameters for channels/signals that are not selected for synchronization.
Select to automatically find a sync slot in the frame.
To specify the sync slot manually, clear . You will also need to set the index and specify the resource block allocation of the sync slot using and .
There must be a unique slot in the Measurement Interval for the frame boundary to be detected correctly. This unique slot can be defined for PUSCH, PUCCH Physical Uplink Control Channel, or SRS Signaling Reference Signal. The Sync Type parameter determines which channel's sync slot is used for frame boundary calculations.
-
Configure remaining per-slot parameters
-
Set PUSCH channel power ()
-
Set DMRS power ()
-
-
Return to Uplink user allocations and configure other channels and signals.
Manually defining PUSCH resource block allocations
-
Select the tab
-
Add PUSCH subframe allocations
Use the , , , and buttons to add a slot allocation for each slot containing PUSCH for the currently selected user.
-
Configure Per-slot Parameters
These parameters are coupled across all slots by default. To set these parameters for each slot allocation individually, clear the check box next to the parameter.
-
Set resource block frequency location (and )
You can interact with the allocations in the grid below by clicking on them. Clicking selects an allocation. Dragging will reposition an allocation. And, dragging the circular handles at the corners will resize an allocation.
-
Set modulation type ()
- Set PUSCH channel power ()
- Set
The remaining are configured in the following steps.
-
-
Configure frequency hopping
-
Set frequency hopping type ()
-
Specify whether to use or frequency hopping ()
-
Set
-
Set
-
Set per-slot parameter when this PUSCH channel uses frequency hopping.
Set per-slot parameter when manually specifying physical resource blocks for frequency hopped signals.
-
-
Configure Demodulation Reference Signal (DMRS) parameter auto-calculation
-
Select
-
Set
-
Set
-
Set
To specify DMRS parameters manually, clear the parameter and set , , and per-slot parameters. These DMRS parameters will apply to all PUSCH slot allocations unless you clear the check box to the left of the parameter name.
-
-
Configure sync slot
Select to automatically determine the sync slot. The demodulator will choose a unique slot from the slot allocations. When there is more than one unique slot defined, the demodulator will use the one with the highest correlation.
To manually specify which slot to use as the sync slot, clear and set the index.
-
Return to Uplink user allocations and configure other channels and signals.
See Also